{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the outside diameter and depth of the 9001K68 / 9001K685 mushroom button guards?

Issue:
9001K68 / 9001K685 mushroom button guards dimensions

Product Line:
30mm Class 9001 Type K Harmony Pushbuttons

Environment:
Type K and SK Accessories

Resolution:
Outside diameter: 2.75 inches (70 mm)
Depth: 1.14 inches (29 mm)

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: