{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the replacement operating handle for VCD__ Vario door mounted manual motor control switch?

Issue:
What is the replacement operating handle for VCD__  Vario door mounted manual motor control switch?

Product Line:
VCD02 VCD01 VCD0 VCD1 VCD2

Environment:
All

Cause:
Repair part

Resolution:
The operating handle is KCD1PZ.  It is a red handle with 60mm x 60mm yellow legend plate for single hole mounting. Note that the operating handle will accept up to three padlocks.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: