Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can multiple motors be connected to one solid state soft starter?
Issue:
Can multiple motors be connected to 1 soft starter?

Product Line:
ATS48 ATS22

Environment:
All

Cause:
Application requirement

Resolution:
Yes.
Size the soft starter for the total full load amps of all motors to be connected.
Provide separate overload protection for each motor.

For ATS48: Make sure the CLP parameter in the drC menu is set to OFF.
For ATS22: Make sure SSC parameter in the Adj menu is set to OFF.

Motor connections to the soft starter output should not be made or broken while the soft starter is running.  The resulting sudden change in current will cause problems and possible damage to the soft starter or other equipment.


Schneider Electric Saudi Arabia

Can multiple motors be connected to one solid state soft starter?
Issue:
Can multiple motors be connected to 1 soft starter?

Product Line:
ATS48 ATS22

Environment:
All

Cause:
Application requirement

Resolution:
Yes.
Size the soft starter for the total full load amps of all motors to be connected.
Provide separate overload protection for each motor.

For ATS48: Make sure the CLP parameter in the drC menu is set to OFF.
For ATS22: Make sure SSC parameter in the Adj menu is set to OFF.

Motor connections to the soft starter output should not be made or broken while the soft starter is running.  The resulting sudden change in current will cause problems and possible damage to the soft starter or other equipment.


 

Schneider Electric Saudi Arabia

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Explore more
Range:

Need help?

  • Start here!

    Find answers now. Search for a solution on your own, or connect with one of our experts.

  • Contact Support

    Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Search FAQs

    Search topic-related frequently asked questions to find answers you need.

  • Contact Sales

    Start your sales enquiry online and an expert will connect with you.

I'd like to receive news and commercial info from Schneider Electric and its affiliates via electronic communication means such as email, and I agree to the collection of information on the opening and clicks on these emails (using invisible pixels in the images), to measure performance of Schneider Electric's communications and to improve them. For more details, please read our Privacy Policy.

  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.