{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are the 9001K51 and 9001K52 Closing Plates Metal or Plastic?
Issue:
Clarifying is the closing plates are metal or plastic

Product Line:
9001 30mm

Environment:
North American Products

Resolution:
Both 9001K51 and 9001K52 are plastic.  They do come with a metal ring nut that secures the closing plate to the back of the enclosure.
Meets UL and Nema 1, 2, 3, 4, 4x, 6, 12, and 13.

Schneider Electric Saudi Arabia