{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Are output filters and line reactors the same on VFDs?

Issue:
Output filters vs Line reactors

Product Line:
Drives.

Environment:
N/A

Cause:
Product features.

Resolution:
No. Output filters and Line reactors are not the same thing. (Load reactor if applied to the output)
Filters reduce DV/DT at the motor by filtering high frequencies. This helps protect the motor.
Line reactors add impedance to the line. This reduces current distortion between the drive and motor if applied to the output. It reduces current distortion on the line when applied to the line side of the drive.
See the information for the specific device for additional details.

Filter info at: http://www.transcoil.com/#klc
Reactor info at: https://mtecorp.com/products/reactors/

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: