{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the range for the analog output for motor current for the Altivar 71 or 61 drives?
Issue:
Altivar 71 or 61 analog output range for motor current.

Product Line:
ATV61 and ATV71

Environment:
All

Cause:
Analog output to show motor current is 2 times the drives rated  nameplate motor current.

Resolution:
The range is 0 to 200% of the drive nameplate current.
You can scale this output by going into the Input and outputs section menu 1.5
Find the AO1 that is assigned to motor current and set he max scale to 50% this will give you the output of 1X the drives motor current on the analog output.

CTA-ID : 2029689

Schneider Electric Saudi Arabia