Search FAQs
Are explosion proof enclosures available for GV manual motor starters.
Issue:
NEMA 7/9 rated enclosure for GV manual motor starters
Product Line:
Tesys GV Motor Starters and Protectors
Environment:
TeSys™ GV Manual Starters and Protectors
Resolution:
No hazardous duty enclosures are available for the GV product line.
For explosion proof applications consider the Class 2510 Type M or Type T offering.
NEMA 7/9 rated enclosure for GV manual motor starters
Product Line:
Tesys GV Motor Starters and Protectors
Environment:
TeSys™ GV Manual Starters and Protectors
Resolution:
No hazardous duty enclosures are available for the GV product line.
For explosion proof applications consider the Class 2510 Type M or Type T offering.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: