{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the part number for the door kit for an I-Line HCWM548612U?

Issue:
What is the part number for the door kit for an I-Line  HCWM548612U?

Product Line:
I line panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
The door kit part number is HCW86D. This can be installed on the HCW86TS or HCW86TF 4-pc trim.


CTA-ID : 2031605

Schneider Electric Saudi Arabia