{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the minimum Ohms for DB resistor for Altivar 71 drives?
Issue:
Altivar 71 DB minimum resistor

Product Line:
ATV71

Environment:
All

Cause:
DB resistor

Resolution:
Minimum Ohms value for DB resistors varies depending on the power and voltage rating of the drives.
It is acceptable to use Dynamic Brake resistor values equal to or greater than the minimum values.
Do not use resistor values less than the minimum ohms listed.
Wattage depends on the desired duty cycle.
See information in the Altivar 71 Catalog and Installation guides for more details.

See table below

Drive part number Minimum
ATV71H..... Ohms
037M3, 075M3 44
U15M3 33
U22M3, U30M3 22
U40M3 16
U55M3 11
U75M3 8
D11M3X, D15M3X 3
D18M3X 4
D22M3X, D30M3X 3.3
D37M3X, D45M3X 1.7
D55M3X 1.7
D75M3X 1.3
075N4, U15N4 56
U22N4 56
U30N4, U40N4 34
U55N4 23
U75N4 19
D11N4 12
D15N4, D18N4 7
D22N4, D30N4 13.3
D37N4 6.7
D45N4, D55N4 5
D75N4 3.3
D90N4 2.5
C11N4, C13N4 1.9
C16N4 1.9
C20N4, C25N4 0.95
C28N4 0.95
C31N4, C40N4 0.63
C50N4 0.63

Schneider Electric Saudi Arabia

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: