Search FAQs
What is the material composition of the Main Bus Bar of the Masterpact ACB?
The material composition used in the Main Bus Bar of the Masterpact Air Circuit breaker (ACB) is shown in the table attached.
Note:
AL/Sn5 means Aluminum connector with Sn5 coated
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: