Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the heat dissipation of the Altivar 61 Drive when it is in Ready state.

The heat dissipation value of the Altivar 61 Drives when in Ready State (RDY - Drive is powered up but motor is not running) depends on the size of the Drive and of the hardware configuration that is the option cards used (like encoder card, IO extension card, controller inside card etc).

Considering 2 option cards (2 * 3.25W) and 1 encoder card (4.25W) the heat dissipation is approximately between 34W and 53 W up to 18.5KW Altivar 61 Drives.
Maximum is 100W for the biggest size of Altivar 61 Drive.

Schneider Electric Saudi Arabia

What is the heat dissipation of the Altivar 61 Drive when it is in Ready state.

The heat dissipation value of the Altivar 61 Drives when in Ready State (RDY - Drive is powered up but motor is not running) depends on the size of the Drive and of the hardware configuration that is the option cards used (like encoder card, IO extension card, controller inside card etc). 

Considering 2 option cards (2 * 3.25W) and 1 encoder card (4.25W) the heat dissipation is approximately between 34W and 53 W up to 18.5KW Altivar 61 Drives.
 
Maximum is 100W for the biggest size of Altivar 61 Drive.

Schneider Electric Saudi Arabia

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Explore more
Range:

Need help?

  • Start here!

    Find answers now. Search for a solution on your own, or connect with one of our experts.

  • Contact Support

    Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Search FAQs

    Search topic-related frequently asked questions to find answers you need.

  • Contact Sales

    Start your sales enquiry online and an expert will connect with you.

  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.