{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is the Automatic adaptation of deceleration ramp feature available in Altivar 61 drive.

Automatic adaptation of deceleration ramp feature is available in Altivar 61 drive.

It assists in prevention of over voltage fault, in case the user has set the deceleration ramp value very low for the high load inertia applications, by automatically adapting the deceleration ramp.
brA [Dec Ramp Adapt.] = Yes (It is a factory default setting).

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: