{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the DC Bus Voltage Threshold at which the Brake IGBT operates in Altivar 71 Drive powered with 220VAC or 415VAC 3 Phase.

Article available in these languages: French, Dutch

The Altivar 71 Drive Braking IGBT operates when the value of DC Bus Voltage is higher than the DC Bus Threshold Voltage OBR. When the value of the DC Bus Voltage is lower than the threshold voltage (Unom_max + 10%), the Braking IGBT/Transistor is switched off.

The Voltage Threshold Values for a Drive working on 220VAC or 415VAC, 3Phase is provided in the attachment.

Note:

OBR is the threshold point where the Braking Transistor switches ON and Unom_max + 10% is the threshold point where the Braking Transistor switches OFF.

Schneider Electric Saudi Arabia

Attachment(s)
Voltage Threshold.pdf [12.14 KB]