Search FAQs
What is the Temperature Threshold at which the Cooling Fan of Altistart 48 Soft Starter start and stop is controlled?
The Temperature Thresholds at which the Cooling Fan of Altistart 48 Soft Starter start and stop is controlled are as follows:
1. Start – Heatsink Temperature > 50°C.
2. Stop – Heatsink Temperature < 40°C.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: