In order to gain access to all the Altivar 31 Drive parameters one of the two conditions will apply:
1. Parameter Access Via Standard Keypad (Integrated LED Display):
Enter the Customer password in parameter Terminal Locking Code (Cod) in Monitoring Menu (Sup).
2. Parameter Access Via Remote Keypad:
a. Enter the Customer password in parameter Terminal Locking Code (Cod) in Monitoring Menu (Sup).
AND
b. Set the Dip Switch called ‘Access Locking Switch’ at the rear portion of the Remote Keypad to ‘Unlock’ position. Refer to the attachment.
Note:
Customer password protection has priority over the switch setting.
Note:
In case the Customer set password is forgotten use the Master password ‘6969’ which resets the customer password and opens access to all parameters.
Released for:Schneider Electric Saudi Arabia