{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the part number for the disconnect handle used on E-Flex Enclosed drives?

Issue:
Cusomer wants to replace a broken or inoperative handle.

Product Line:
E-Flex Enclosed Drives

Environment:
Type 1 and Type 12 - all models and part numbers

Cause:
Disconnect handle part number is not listed in the E-Flex Manual

Resolution:
The part number for the Rotary Disconnect Handle is S29338



CTA-ID : 2051053

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: