{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a cover or guard for the XALK yellow station with 40mm red mushroom head push button ?
Issue:
What is the part number for the cover or guard for XALK174?

Product Line:
Push Buttons and Operator Interface

Environment:
22 mm Harmony Control Stations

Cause:
Product Features

Answer:
There is no cover or guard available for the mushroom head push button. There is a raised area on the front of these XALK enclosures which will not allow
a guard the be mounted flush to the surface.

Schneider Electric Saudi Arabia