{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the 4-position switch used on the M-Flex for Mod F07?

Issue:
Mod F07 Hand-Off-Auto-Comm selector on the M-Flex part number request


Product Line:
ATV61 ATV71 M-Flex Model 6 MCC


Environment:
All


Cause:
Wiring


Resolution:
The Hand-Off-Auto-Comm selector is made up of the following:
KAXZ1M12 Operator Handle
9003K2H0285USX Contact Block
65170-170-41 A-O-H Legend Plate
31164-098-01 COMM Label
ZBZ32 LEGEND PLATE HOLDER

Schneider Electric Saudi Arabia