{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can TeSys T overloads be used on a single phase motor application?
Issue:
TeSys T overloads application assistance

Product Line:
IEC Contactors and Starters

Environment:
TeSys T Overlaod Relays

Cause:
Product Application

Resolution:
Yes. There is a configuration selection for single or 3 phase. If single phase is selected, use the two outer CT windows for the power conductors.

Schneider Electric Saudi Arabia