Search FAQs
For ATV61/71 Ethernet IP (VW3A3316), what is the web page default password?
Issue:
How can I find the default password used to access the ATV61/ATV71 web page when using Ethernet IP Communications?
Product Line:
Altivar Drives
Environment:
Altivar 61, Altivar 71, Altivar 61Q, Altivar 71Q
Cause:
Communication card, Password
Resolution:
There are two passwords.
To get into Monitor and Setup Security:
User Name: USER
Password: USER
To get into Administrator:
User Name: ADMIN
Password: ADMIN
*This is Case Sensitive, All CAPS
How can I find the default password used to access the ATV61/ATV71 web page when using Ethernet IP Communications?
Product Line:
Altivar Drives
Environment:
Altivar 61, Altivar 71, Altivar 61Q, Altivar 71Q
Cause:
Communication card, Password
Resolution:
There are two passwords.
To get into Monitor and Setup Security:
User Name: USER
Password: USER
To get into Administrator:
User Name: ADMIN
Password: ADMIN
*This is Case Sensitive, All CAPS
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: