{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the replacement for a 9001TB contact block?
Issue:
Replacement part number for a 9001TB contact block

Product Line:
Push Buttons and Operator Interface

Environment:
9001K Push Button

Resolution:
Replace with a 9001TAD1 liner and (2) 9001KA1 contact blocks.
Note that the 9001TAD1 is obsolete. The entire operator will need to be crossed to the 9001K line of pushbuttons.

Schneider Electric Saudi Arabia