{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the IP rating for 22mm Push Buttons XB4 and XB5?
Issue:
Clarify the 22mm operator IP rating

Product Line:
Push Buttons and Operator Interface

Environment:
Harmony XB4/XB5 22mm push button

Cause:
Product Specification

Resolution:
As of 2017, all of the XB4 and XB5 push buttons are rated IP66, IP67, IP69, and IP69K or UL Type 4X.

Schneider Electric Saudi Arabia