{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the maximum AIR (or SCCR) for the QMB/QMJ branch switches when used on a DC voltage system?

Issue:
Product Design Features

Product Line:
QMB branch switches

Resolution:
FIRST, VERIFY THAT THE SPECIFIC QMB/QMJ BRANCH SWITCHES HAVE A DC VOLTAGE RATING AND THIS SHOULD BE MARKED ON THE SWITCH WIRING DIAGRAM.


The maximum short circuit current rating for the QMB/QMJ branch switches when used on a DC voltage system is 10 kAIC. This applies to all DC voltage systems (see wiring diagram of switch to confirm if rated for DC; 250 Vdc maximum).

Schneider Electric Saudi Arabia