{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the difference between 9001KYG1Y1 and 9001KYG1Y2?
Issue:
9001KYG1Y1 and 9001KYG1Y2 Difference

Product Line:
30 mm Enclosures

Environment:
9001KY/SKY Control Stations

Resolution:
9001KYG1Y1 includes a push/pull operator 9001KR9R
9001KYG1Y2 includes a turn to release operator 9001KR16.

Both have the same 9001KYG1Y enclosure with the same 9001KA3, one normally closed contact block.

Schneider Electric Saudi Arabia