{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

RS-485 Converters for the UPS SmartSlot Building Management Card (AP9622)

Issue



RS-485 Converter Compatibility for AP9622 Building Management Modbus/JBUS UPS SmartSlot card

Product Line

  • UPS Device Management
    • AP9622 Building Management Modbus/JBUS UPS SmartSlot Card

Environment



AP9622 installations requiring RS-232 to RS-485 converter to work with various Building Management Systems

Cause



The AP9622 card supports RS-232 Modbus/JBUS output. Users may require RS-485 adapters to work with an existing Building Management System. Refer to compatibility list below.

Resolution




The Building Management Integration Card (AP9622) will work with the following RS-232 to RS-485 converters:
  • B&B Electronics P/N: 485OT9L*
*Item is currently discontinued per B&B. The recommended replacement is 4WSD9OTB but it has not been tested with the AP9622.
  • B&B Electronics P/N: 485LP9TB
Below is an example diagram for a 485LP9TB application:


Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: