Search FAQs
No metering outlets detected" or "Lost Communication" error(s) on standalone AP84XX or AP86XX Metered By Outlet Rack PDUs
Issue
"No metering outlets detected" or "Lost Communication" error(s) on standalone AP84XX or AP86XX Metered By Outlet Rack PDUs.
These can show on the web interface or event log of the PDU.
Event Log: Rack PDU: Component communications lost with Phase Meter.
Web UI (v5.X.X):
Web UI (v6.X.X):
Product Line
- Rack Power Distribution
- AP86XX - Switched Rack PDU with Metering By Outlet
- AP84XX - Metering By Outlet Rack PDU
Environment
- All serial numbers
- All firmware versions
- PDU standalone configurations (not using Network Port Sharing)
Cause
For proper operation of your standalone Metering By Outlet Rack PDU (AP86XX or AP84XX), you must install the terminator included with your Rack PDU either the IN or OUT port. If this terminator is not connected, you will receive the following error or similar: No metering outlets detected; Lost Communication with device; Lost Communication with Phase Meter.
Resolution
Note: For units manufactured December 2012 and later, the lower profile terminator will now come pre-installed in either the IN and OUT port. Installation should be verified if you see the aforementioned communication errors though.
For older units or if the pre-installed terminator was removed, install the terminator included with your Rack PDU documentation and literature, part number 0W05545A which is a low profile terminator or the older, larger 0W04161A. Please see below.
If you have lost or misplaced your terminator, please contact technical support in your region for replacement options.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: