{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to reduce the Battery Charge Capacity for Smart-UPS VT
The SUVT UPS normally has a charging current of 10% (FW 6.8 could be as high as 20%) of the capacity of the UPS. However there are cases where it may be necessary to limit or reduce this current. The reasons for this could be for example capacity limitations during Generator Operation or a requirement to reduce temperature in the event of problems with Air Conditioning.

Note: When this function is active, no fault will appear on the SUVT UPS.

The attached document describes this in greater detail.

Schneider Electric Saudi Arabia

Attachment(s)
Charge Limiting for SUVT UPS.doc [166.5 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: