Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to test which battery is bad (internal or external?) on a Smart-Ups XL model

Article available in these languages: Russian

Issue:
How to test which battery is bad (internal or external?) on a Smart-Ups XL model

Product Line:
Smart-UPS

Environment:
All legacy (SU, SUA, SUM, SURT) Smart-UPS models with an "XL" suffix, All Serial Numbers

Cause:
Standard Operation

Resolution:

When a legacy Smart-UPS indicates "replace battery", it is referring to the full battery string. The UPS does not have the ability to test specific modules or external battery frames individually. When the UPS tests the batteries, it is looking for the rate that voltage drops over time for a given load. There is not a way to easily replicate this using a voltmeter. You should defer to the results of the UPS self test with a fully charged battery and the normal load attached. The self test will run once every two weeks by default.

Furthermore, it is important to never mix mix old and new battery cartridges within the same Smart-UPS system. When batteries are replaced, you should replace all the battery modules (internal and external) at the same time. In addition, if you add more external batteries to an existing unit, you should replace the existing batteries at the same time if they are more than 1 year old. For more information on this, refer to FAQ #FA317828 "Can I mix old and new batteries in a Smart-UPS?"

Batteries typically last 3-5 years in an appropriately cooled (68°F-77°F / 20°C-25°C) environment.

Schneider Electric Saudi Arabia

How to test which battery is bad (internal or external?) on a Smart-Ups XL model

Article available in these languages: Russian

Issue:
How to test which battery is bad (internal or external?) on a Smart-Ups XL model

Product Line:
Smart-UPS

Environment:
All legacy (SU, SUA, SUM, SURT) Smart-UPS models with an "XL" suffix, All Serial Numbers

Cause:
Standard Operation

Resolution:

When a legacy Smart-UPS indicates "replace battery", it is referring to the full battery string. The UPS does not have the ability to test specific modules or external battery frames individually. When the UPS tests the batteries, it is looking for the rate that voltage drops over time for a given load. There is not a way to easily replicate this using a voltmeter. You should defer to the results of the UPS self test with a fully charged battery and the normal load attached. The self test will run once every two weeks by default. 

Furthermore, it is important to never mix mix old and new battery cartridges within the same Smart-UPS system. When batteries are replaced, you should replace all the battery modules (internal and external) at the same time. In addition, if you add more external batteries to an existing unit, you should replace the existing batteries at the same time if they are more than 1 year old. For more information on this, refer to FAQ #FA317828 "Can I mix old and new batteries in a Smart-UPS?"

Batteries typically last 3-5 years in an appropriately cooled (68°F-77°F / 20°C-25°C) environment. 

Schneider Electric Saudi Arabia

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Explore more
Range:

Need help?

  • Start here!

    Find answers now. Search for a solution on your own, or connect with one of our experts.

  • Contact Support

    Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Search FAQs

    Search topic-related frequently asked questions to find answers you need.

  • Contact Sales

    Start your sales enquiry online and an expert will connect with you.

I'd like to receive news and commercial info from Schneider Electric and its affiliates via electronic communication means such as email, and I agree to the collection of information on the opening and clicks on these emails (using invisible pixels in the images), to measure performance of Schneider Electric's communications and to improve them. For more details, please read our Privacy Policy.

  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.