{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

InRow Entering Fluid Temp threshold is not alarming

Issue:
InRow Entering Fluid Temp threshold is not alarming

Product line:
InRow

Environment:
Data Center Cooling

Cause:

Resolution:
In the newest firmware ACRC 372 and higher the entering fluid temp alarm threshold violation will not be reported unless two conditions are met. The unit has a >=40% valve position opening, and the entering temperature is above the threshold.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: