{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the FM Water Flow Switch Alarms description?
Issue: FM Water Flow Switch Alarm

Product line: FM

Environment: Data Center Cooling

Cause:

Resolution:
Here are the conditions for producing a flow switch alarm:

Note that the flow switch opens when there is no flow.

If you have selected a flow switch = MC/CW
If the flow switch is open and the MC/CW valve is a 3 way valve then an alarm will be generated.
If the flow switch is open and the MC/CW valve is a 2 way valve and the valve is open more than 30% then an alarm is generated.

If you have selected a flow switch = DX/ECON
If the flow switch is open and [the coil configuration = ECON or the water regulation valve = 3 way or (the water regulation valve = 2 way and the water regulation valve is open more than 30%)] then an alarm is generated.

Schneider Electric Saudi Arabia

Explore more
Range:
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product: