Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Can your InRow Cooling Auto-Start after a Power Failure

Article available in these languages: Spanish

Issue:
Can your InRow Cooling Auto-Start after a Power Failure
 
Product line:
InRow
 
Environment:
Data Center Cooling
 
Cause:
 
Resolution:
The InRow RC, RD, RP and SC will start automatically if the power is restored after a power failure. The unit will go to its last known state, ie if the unit was in standby, the unit would return to standby, or if the unit is on, the unit would return to the on state.

It is also possible to configure a Start up Delay of 0 to 999 seconds.

That can be done from:
  1. The Display: Configure Unit>General> Startup Delay
  2. The Network Management Card Interface: Unit>Unit Configuration> Startup Delay

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: