{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
InRow RC Standard and Optional Features
Issue: InRow RC Features

Product line: InRow RC

Environment: Data Center Cooling

Cause:

Resolution:
1-The Standard Features of the InRow Rc Coolling Unit are as follow:

Variable Speed Fans
Shutdown Input/Alarm Output
Chilled Water Flow Meter
2-way/3-way Floating Point Valve
Dual A-B Power Feed
Washable Filter
Pipe Adapters
Top or Bottom Piping
Condensate Pump with Dual Float Switches
Network Management Card
Remote Temp Sensor
Microprocessor Controller

2-Other Optional Features or accessories are as follow:

Cable Leak Detector
Baying Kit InRow RC to NetShelter VX rack
30% ASHRAE 52.1 Filter (MERV 8 per ASHRAE 52.2)
NetShelter SX Height Adapters
NetShelter VX Height Adapters
Power Trough (Overhead power distribution between racks)
Data Partion Trough (Allows removal of RC unit without disrupting cabling)

Schneider Electric Saudi Arabia