{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Symmetra Power Array redundancy alarm is limited to N+2

Issue

Symmetra Power Array has a maximum redundancy alarm limit of N+2.  The user cannot set this alarm to a value greater than 2.  This means that if the user


Product Line

Symmetra Power Array


Environment

All serial ranges


Cause

The system is unable to support a value greater than 2 for the user configurable redundancy alarm.


Resolution

The system is not capable of this function.

Please Note:
The Symmetra can report on current redundancy levels greater than N+2, such as via the PowerView Status menu or Network Management Card, etc.  The system is simply not capable of alarming when the redundancy limit falls below N+3.  This is not considered a typical use case anyway.



Schneider Electric Saudi Arabia