Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
No power output from the Matrix-UPS L14-30 or 5-15 receptacles (MX3000/5000)

Issue

Matrix-UPS is not providing any output power to the receptacles on the rear of the UPS.


Product Line

Matrix-UPS


Environment

All


Cause

There is an ON/OFF circuit breaker switch located on the back plate of the Matrix-UPS IU (Isolation Unit, lower half of the Matrix-UPS) just above the NEMA L14-30 receptacle. This breaker controls the UPS output to the L14-30 receptacle (as well as the NEMA 5-15 receptacles on the Matrix-UPS 3000 model only). On the Matrix-UPS 5000, this switch controls the L14-30 receptacle only. If the Matrix-UPS is powered on and there is no output to the L14-30 receptacle (or any of the 5-15 receptacles on a Matrix-UPS 3000) check this switch to ensure that it is set to ON (to the right). This symptom is often experienced on a new installation.


Resolution

Close the breakers to restore power to the receptacles.  If the breaker has tripped while the unit was in service, this was due to an overload to the circuit by loads downstream of the Matrix-UPS. Evaluate the circumstances and correct by reducing the number of connected devices.



Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.