Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Are Symmetra LX Intelligence Modules Universal?


Yes.  There are no country or region specific versions of the SYMIM5.  It is universal and can be used in both split-phase (208/240V) Symmetra LX models as well as 3:1 / 1:1 (220/230/240V or 380/400/415V) Symmetra LX models.


Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: