{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
DIN Connector Pin Outs For the Netbotz Appliances
Issue:
DIN Connector Pin Outs For the Netbotz Appliances

Product Line:
NetBotz

Environment:
NetBotz version 1 and 2 cables

Cause:
Pin-out specifications.

Resolution:
DIN Connector Pin Outs

-NetBotz does not release the pin outs for the DIN connectors for any NetBotz Appliances.

-To address this issue, NetBotz sells a standard dry contact cable that is our DIN connector one end and two bare dry contact style wires on the other.

-This cable is provided to allow customers to attach our NetBotz Appliances to any dry contact type connection without having to have the DIN connector pin outs.




Schneider Electric Saudi Arabia