{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

NetBotz Room Monitor 355/455 | POE Power Specifications

Issue:
NetBotz Room Monitor 355/455 POE Power Specifications

Product Line:
NetBotz

Environment:
NetBotz Version 3 using POE

Cause:
POE specifications

Resolution:

The NetBotz 355 and 455 are Class 0 POE devices.

The IEEE standard 802.3 for supplying power over Ethernet allows the device providing power to use a voltage between 36–57 V DC. The nominal voltage is 48 V with a current of 10–400 mA, subject to a maximum load power of 15.40 Watts.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: