{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Are APC Cat 6 Patch Panels color coded for 568B or 568A?

Issue:
The installer needs to know the color code on the rear of the Cat 6 patch panel.
Product Line:
Cables and Connectivity Solutions, Patch Panels
Environment:
CAT6PNL-24, CAT6PNL-48
Cause:
Installers need to know if the patch panel has the color code they require.
Resolution :
The CAT6PNL-xx series of Patch Panels have both 568B and 568A color codes.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: