Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to change the lock and key in a NetShelter SX or SV cabinet? Users may want some, or all, their cabinets to be keyed differently.

Article available in these languages: Spanish

Issue:
Customers need to know what type of locks are available, how can they be purchased and how they're installed.

Product Line:
NetShelter SX, NetShelter SV

Environment:
All versions and serial ranges.

Cause:
A request has been made to replace the existing locks, or to replace the standard locks with uniquely keyed locks.

Resolution:
See Attached

Schneider Electric Saudi Arabia

Attachment(s)
20130408 Uniquely Keyed Locks for Netshelter SX Enclosures Rev6.pdf [356.4 KB]