{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Will the NetShelter SX leveling feet support the full weight of the cabinet and its contents?

Issue:
Can the full weight of the NetShelter cabinet rest on the leveling feet?
Product Line:
NetShelter SX
Environment:
All versions and serial ranges.
Cause:
Cabinets are leveled using the leveling feet so  they need to bear the full weight of the cabinet and it's contents. (static load rating)
Resolution:
Yes, the leveling feet can support the cabinet up to the rated static load rating of the cabinet.
FAQ FA158656 also contains information regarding shipping load, dynamic load and static load ratings.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: