Search FAQs
Is there a roof available for the AR3100 which is solid and does not have open cable access holes?
Issue:
There may be a need for a solid roof on the cabinets.
Product Line:
NetShelter SX
Environment:
All versions and serial ranges.
Cause:
A more secure roof may be required for installations such as PCI.
Resolution:
The WAR7210 can be used where high security is required. It is compatible with the following models: AR3100, AR3104, AR3105, AR3200 and AR3107.
For more information and a photo please see the attached file.
There may be a need for a solid roof on the cabinets.
Product Line:
NetShelter SX
Environment:
All versions and serial ranges.
Cause:
A more secure roof may be required for installations such as PCI.
Resolution:
The WAR7210 can be used where high security is required. It is compatible with the following models: AR3100, AR3104, AR3105, AR3200 and AR3107.
For more information and a photo please see the attached file.
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: