Search FAQs
Does the AR2144BLK or AR2145BLK NetShelter VX Seismic have leveling feet or castors available as an accessory?
Issue:
A customer may ask if castors are an accessory for our NetShelter VX cabinet.
Product Line:
NetShelter VX
Environment:
All versions and serial ranges.
Cause:
Castors can be used to move the cabinet much eaqsier.
Resolution :
The NetShelter VX cabinets do not offer castors as an accessory. These cabinets are approved for NEBS GR-63-CORE seismic installation, which does not include the use of castors.
Also see attached document.
A customer may ask if castors are an accessory for our NetShelter VX cabinet.
Product Line:
NetShelter VX
Environment:
All versions and serial ranges.
Cause:
Castors can be used to move the cabinet much eaqsier.
Resolution :
The NetShelter VX cabinets do not offer castors as an accessory. These cabinets are approved for NEBS GR-63-CORE seismic installation, which does not include the use of castors.
Also see attached document.
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: