{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the electrical specifications of the power supply for ACF600?
Issue:
Customers may need electrical specifications for the ACF600 power supply.

Product Line:
NetShelter AV

Environment:
ACF600 all versions and serial ranges.

Cause:
Review of the electrical specifications of the ACF600 power supply.

Important Note: This unit should only be used with regulated power supplies. If not using a regulated power supply and using an unregulated adjustable voltage power supply such as the PS-300 or PS-500, the power supply should then possibly require a setting of 9V, although this is not optimal. The issue is that often times unregulated power supplies will supply higher voltage when not under load or under a light load. Higher voltage will not damage the unit, it simply will not perform within the specifications.
Connection:          2-Pin FastWire Power System (Ensure proper polarity - Tip to +)
Voltage:               12V DC ***See “Important Note” above***
Current - Amps:    Output Rated at 2 Amps (Max)


Resolution:
see attached file

Schneider Electric Saudi Arabia

Attachment(s)
20120321 ACF600 Power Supply Info Rev2.pdf [410.31 KB]