{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is a service loop required on install of a TVSS SurgeArrest Panel Mount device?
Issue:

The Panel Mount SurgeArrest is hardwired so there is the question of whether or not a service loop is required by the NEC. According to the National Electric Code, Article 300 section 14.


Product Line:

All TVSS Panel Mount Devices


Environment:

All TVSS Panel Mount Devices


Cause / Resolution:

Length of Free Conductors at Outlets, Junctions, and Switch Points. At least 6 in. (152 mm) of free conductor shall be left at each outlet, junction, and switch point for splices or the connection of fixtures or devices.

Exception: Conductors that are not spliced or terminated at the outlet, junction or switch point.""

The Panel Mount Protectors do not fall under these three items, therefore no service loop is required by the NEC for wiring internal to our product. However, when connected to the Circuit Breaker inside the AC Panel, the wires will have to have a 6"" Service loop."

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
move-arrow-top
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.