{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: Back-UPS CS, RS & XS - Manual Adjustment for Sensitivity

Article available in these languages: Spanish

Issue:

UPS will not operate on utility power or may be clicking between utility and battery power.


Product Line:

Back-UPS RS/XS & Back-UPS CS (4-LED Interfaces)


Environment:

All models & serial numbers


Cause:

This may be caused by one of the following conditions;
  • Low Voltage / Sag
  • Black-out / Power Outage / Power Interruption
  • High Voltage / Over-Voltage / Voltage Swell
  • Frequency is out of range
  • Total Harmonic Distortion

Resolution:

The following video details the process for manually adjusting the Back-UPS RS & XS or Back-UPS CS system's AC Input Sensitivity.

Schneider Electric Saudi Arabia