{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Configuring Microsoft Windows 7, 8, 10, & 11 Windows Server 2008, 2012, 2016, 2019, & 2022 to safely shutdown without using APC's PowerChute software.

Issue:
How to configure Microsoft Windows 7, 8,10, & 11 Windows Server 2008, 2012, 2016, 2019 & 2022 to safely shut down without using APC's PowerChute software.

Product:
APC branded UPS with Serial Connections

Environment:
Microsoft Windows 7, 8,10, & 11 Windows Server 2008, 2012, 2016, 2019 & 2022

Cause:
Informational

Solution:

Microsoft Windows 7, 8,10, & 11 Windows Server 2008, 2012, 2016, 2019 & 2022 do not have a native serial UPS shutdown. For a serial UPS, use the supported PowerChute software (PowerChute Business Edition / PowerChute Serial Shutdown.

For any USB-connected UPS, these OS have some configuration for shutdown if you do not want to use the supported APC software options. Once a USB UPS is connected, the OS adds a configuration similar to that of a laptop with an onboard battery. Once this happens, you can set up a desktop or server's power options in the same way as a laptop.

Please review the attached PDF for instructions:

Also, if the native battery shutdown options are not displayed after uninstalling PowerChute software, please review Video: What to do if the system is missing native shutdown battery options / How to restore HID UPS device driver.

Schneider Electric Saudi Arabia

Attachment(s)
How to configure Microsoft Vista, Windows 7, 8 , 10 Server 2008, 2012, 2016, 2019 Native Shutdown.pdf [1.89 MB]