{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Starting and Stopping PowerChute Network Shutdown on Windows Server Core

Issue:
How to start and stop PowerChute Network Shutdown on Windows Server Core

Product:
PowerChute Network Shutdown Versions 2.2.3 and above

Environment:
Windows Server Core

Solution:

To start the PCNS service manually after it has been deliberately stopped, use either command below:

Note: "n" stands for the instance number, if only one instance was installed n=1 Each instance was it own number PCNS 2.2.3, 2.2.4 and 2.2.5 can have up to 3 instances. PCNS 3.X and 4.X have 1 instance only so the entry is PCNS1.

sc start PCNSn

net start  PCNSn

To  stop the PCNS service when it is running, use either command below:

sc stop PCNSn

net stop PCNSn

To check if  PCNS service is running on Windows Service Core, use either command below:

sc query PCNSn #This command will only list the PCNS service and show if the service is started or stopped.

net start # This command without argument will list all services running on the system.

sc query # This command without argument will list all services running on the system.

Schneider Electric Saudi Arabia

Explore more
Category:
Software
Explore more
Category:
Software
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.