{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Manual Removal of PowerChute Personal Edition on Windows Systems

Issue:
Uninstallation of PowerChute Personal Edition fails or is incomplete.

Product:
PowerChute Personal Edition (PCPE)

Environment:
Windows XP, Vista, Windows 7, Windows 8, Windows 10

Cause:
Incomplete or failed uninstallation

Solution:

NOTE: Editing the system registry improperly can cause system damage. Schneider Electric is not responsible for any consequence caused by editing of the system registry.

Please review the corresponding Microsoft Kbase concerning the system registry before proceeding https://support.microsoft.com/en-us/help/322756/how-to-back-up-and-restore-the-registry-in-windows

You will want to kill the PowerChute.exe, apcsystray.exe, mainserve.exe, and dataserv.exe processes if running before you do the following steps

1. From the installation directory in Explorer

(e.g. 32 Bit - C:\Program Files\APC\APC PowerChute Personal Edition

64 Bit - C:\Program Files (x86)\APC\APC PowerChute Personal Edition remove the entire contents from the first 'APC' down, that is assuming you used the default path and you do not have any other APC products installed.

2.a In the Registry (open by going to Start->Run->type 'regedit') a. go to the

32 bit - 'My Computer\HKEY_LOCAL_MACHINE\Software\APC' key.

64 bit - 'My Computer\HKEY_LOCAL_MACHINE\Software\Wow6432Node\APC.

If you do not have any other APC products installed delete the entire APC key, otherwise just delete the APC PowerChute Personal Edition key.

2.b Go to the registry

32 Bit - My Computer\HKEY_LOCAL_MACHINE\Software\Microsoft\Windows\CurrentVersion\Uninstall

64 Bit - My Computer\HKEY_LOCAL_MACHINE\Software\Wow6432Node\Microsoft\Windows\CurrentVersion\Uninstall and then search for PowerChute Personal Edition.
This should return a key with the following contents:
DisplayName
UninstallString.
Remove the entire key where the match occurs.
*Note: Keep track of the 'name of the string', it should be something like {F1486DE6-CC2E-48C0-AD20-C2C142FA1636}. The name string will be depend on what Windows installer assign to it.

64 Bit - running PowerChute Personal Edition 3.1 the uninstaller is in My Computer\HKEY_LOCAL_MACHINE\Software\Wow6432Node\Microsoft\Windows\CurrentVersion\Uninstall\APC

2.c Go to registry on both 32 bit and 64 bit machines - 'My Computer\HKEY_LOCAL_MACHINE\Software\Classes\Installer\Products\'

search for 'PowerChute Personal Edition'.

This should return a key with the following content:

ProductName

Remove the entire key where the match occurs

3. If there is still an issue run Microsoft Fix It

NOTE: Once PowerChute has been removed you may need to re-enable HID USB driver to enable Native Power Option i.e. battery icon in the systray. See Schneider Elecric FAQ FA159743 for assistance.

Schneider Electric Saudi Arabia

Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: