Issue:
Will the remote VW3A1101 HMI have speed control over the drive if FNOD is set to 3?
Product Line:
Altivar 212
Environment:
All
Cause:
Configuration
Yes the HMI`s wheel will have speed control over the drive.
Released for:Schneider Electric Saudi Arabia