{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the operating temperature range of the ATS01 soft starters?

Issue:
What is ATS01 soft starter operating temperature?

Product Line:
ATS01

Environment:
All series

Causes:
N/A

Resolution:
The ATS01 soft starters are rated for use in ambient temperatures ranging from -10C (14F) to +40C (104F).  The starter can be used up to 50C (122F) by derating the current by 2% per degree C above 40C.

The obsolete ATS01N2**LY were rated for use in ambient temperatures ranging from 0C (32F) to +55C (131F).

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: